5-Phase CVD Series Fully Closed-Loop Stepper Motor Driver

The CVD Series driver, which utilizes a fully closed-loop control system, enables precise positioning by integrating with an external sensor. This allows for high-precision position correction using feedback from the external sensor. If the desired position is not initially achieved, the control system seamlessly transitions from open-loop to fully closed-loop control, and then performs the necessary position correction.

5-Phase Stepper Motors



©2025 - ORIENTAL MOTOR USA CORP. - All Rights Reserved