Everything You Need to Know About Stepper Motors

The Powerful Ability of Highly Reliable Stepper Motors

Stepper motors are often misconceived as the lesser of servo motors, but as a matter of fact, they are highly reliable just like servo motors. The motor operates by accurately synchronizing with the pulse signal output from the controller to the driver, achieving highly accurate positioning and speed control. Stepper motors feature high torque and low vibration at low-speeds, ideal for applications requiring quick positioning in short distance.

Everything You Need to Know About Stepper Motors

"Stepper motors? Servo motors must have better performance." This is a typical response when asked about stepper motors. Obviously there is a major misconception about stepper motors. In fact, stepper motors have been used in various types of applications such as advanced equipment and accessible automated instruments. The reasons why stepper motors have been continuously chosen are explained in this article. Some readers may say that they have never seen a stepper motor before. Stepper motors have been used in many applications and industries as the motor solution for drive systems requiring high accuracy control, such as factory automation (FA), manufacturing equipment for semiconductor, FPD and solar panel, medical devices, analytical instruments, precision stage, financial systems, food packaging machines, and aperture diaphragm adjustments for cameras.

Why do you use a stepper motor?

Easy to use: 34%
Inexpensive: 17%
Simple operations:16%
No need for tuning: 12%
Other: 21%
*# of questionees: 258 (multiple answers allowed)/ researched by Oriental Motor

Key Points: Ease-of-Use, Simple Operations and Low Cost

According to the survey of stepper motors users, many favor stepper motors for their "ease-of-use," "simple operations", and "low cost" derived from the structure and system configuration. It makes sense that many users find such positive aspects in stepper motors, thanks to the simple structure and system configuration. However, some readers may be skeptical about the actual performance of the motor in terms of its accuracy and torque. It is not easy to fully grasp the whole idea unless there are comparison examples against other control motors such as servo motors. By knowing the characteristics and taking on different approaches based on required operations, stepper motors certainly can reduce the cost of the equipment. The characteristics and technical information of stepper motors are explained below:

Impressive "Stopping Accuracy." Moves Quickly in the "Low / Mid-Speed Range"

Stepper motors have remarkable stopping accuracy, and accurate control with open-loop is possible. For example, when using the RK II Series for positioning of a rotating table, its stopping accuracy is within ±0.05° (with no load). Because stopping position errors do not accumulate between steps, high accuracy positioning is possible. The structure of the stepper motor, which requires no encoder, allows for the simple drive system and low cost.

Point 1
Fantastic Stopping Accuracy

For example, when converting stopping accuracy ±0.05° of a stepper motor to the ball screw mechanism:

Operating Conditions:
• Motor: RK II Series

• Lead of ball screw: 10mm

Stopping Accuracy: ±1.4µm

Generally, accuracy of a ground ball screw type is ±10µm. When using a rolled ball screw type, its accuracy declines to ±20µ m, indicating that the stopping accuracy of a stepper motor is much higher than that of ball screw types.

Stepper Motor Stopping Accuracy Example

High torque within the low / mid-speed range is another great feature of stepper motors. One of the main features of servo motors is to generate flat torque from mid to high speed ranges. Servo motors are suitable for long-stroke operations (many rotations). On the other hand, torque characteristics of stepper motors are not flat. The torque curve within the low / mid-speed range tends to become very high, while becoming very low in the high speed range. Besides the stable rotations in the low speed range, which servo motors struggle with, stepper motors can offer high torque within the required speed range for short-stroke operations (less rotations), thus they are suitable for selecting the desired step angle for multiple rotation tables and inching applications. This is due to the short positioning time for the short-stroke operation, thus the motor decelerates and stops before reaching the maximum speed. In other words, high-speed characteristics are usually not required.

High Responsiveness and Excellent Synchronization

The third remarkable feature of stepper motors is responsiveness. The open-loop control, which sends one-way commands to the motor, has a high followup mechanism toward commands. While servo motors, which wait for feedback from the encoder, tend to have "delays" with commands, stepper motors operate synchronously with a pulse. Therefore, there are very few "delays," resulting in excellent response. For this reason, stepper motors are suitable for applications that require synchronous operations of multiple motors. One example is a board transferring application that requires two conveyors, with one motor mounted respectively, to transfer boards in between the two conveyors.

Point 2
Excellent Low / Mid-Speed Range!

Example: Torque of a motor frame size 85 mm is equivalent to a rated torque of a 400 W servo motor when 1000 r/min.

Torque in an even lower speed range can be up to 5 times higher. For a shortdistance positioning, having high torque in the low / mid-speed range is essential.

RKII Torque Chart

Point 3
High Responsiveness!

Stepper Motor Open Loop vs Servo Closed Loop

Suitable Applications

Other than an inching application with frequent starting and stopping, stepper motors are suitable for positioning of image check processors that dislike vibrations, cam drives that would be difficult to adjust with servo motors, and low rigidity mechanisms such as a belt drive. Furthermore, cost is reduced significantly by replacing a ball screw drive to a belt drive.

Stepper Motor Application Examples

Advantage of Great Features

Besides cost reduction, stepper motors have many advantages in terms of performance. The following chart shows the converting torque of the RKII Series example to that of typical servo wattage ranges. Further down, detailed information on stepper motors, such as basic structure, system, and example applications, is introduced for more information on stepper motors.

Stepper Motor Output Chart

Basics of Stepper Motors

Operation & Structure

A stepper motor rotates with a fixed step angle, just like the second hand of a clock. Highly accurate positioning can be performed with open-loop control thanks to the mechanical structure within the motor.

Accurate Positioning (Number of Steps)

While having full control of rotation and speed, the simple structure of stepper motors is achieved without using electrical components, such as an encoder within the motor. For this reason, stepper motors are very robust and have high reliability with very few failures. As for stopping accuracy, ±0.05° (without cumulative pitch errors) is very accurate. Because positioning of stepper motors is performed by open-loop control and operated by the magnetized stator and magnetic rotor with small teeth, stepper motors have a higher follow-up mechanism toward commands than that of servo motors. Also, no hunting occurs when stopping stepper motors. They are also excellent in belt drives, which have low rigidity.

Useful for Speed Control and Position Control

When pulses are input to a driver through a pulse generator, stepper motors position according to the number of input pulses. The basic step angle of 5-phase stepper motors is 0.72° and 1.8° for 2-phase stepper motors. The rotating speed of the stepper motor is determined by the speed of the pulse frequency (Hz) given to the driver, and it is possible to freely change the motor rotation by simply changing the number of input pulses or frequencies to the driver. Stepper motors not only serve as position control motors, but also as speed control motors with high synchronization.

Stepper Motors Uses:

• High frequency, repetitive positioning of fixed step angles
• Positioning that requires long stopping time due to width adjustment, etc.
• Fluctuating loads and changing rigidity
• Positioning that divides 1 cycle
• Motor shafts that requires synchronous operation

Stepper Motor Operation Structure

Operating System

Simple Control With No Sensor or Feedback

Because it is possible to perform accurate positioning and position control while synchronizing with the number of command pulses and speed, there is no need for devices, such as a sensor, for positioning. Therefore, the entire system is simple to build. If advanced control, such as an interpolation operation, is not required, the built-in controller function type driver is recommended. Cost is reduced by eliminating controllers, such as a pulse generator and PLC positioning modules.

Built-in Sensor Closed-Loop Type

Although high accuracy positioning is possible with open-loop control, what would happen if a problem occured? In order to avoid such pitfalls, an encoder type or built-in sensor closed-loop control type motor (AR Series) can be used.

Stepper Motor Operating System

Can the Cost be Further Reduced?

The common issue among design engineers is cost reduction. Is there really no way to further reduce cost? To find out a cost reduction test, with specification enhancements, was conducted based on the ball screw mechanism. The following explains the details of the test:

Mission

Linear Motion Mechanism

1. Further Increase Speed
2. Further Reduce Cost

[Conditions of the Originally- Planned Equipment] Mechanism: Ball Screw + Servo Motor Conditions such as a load, speed, and lead, shown on the right, are determined based on the servo motor attached with ball screws and steel plate.

Stepper Motor Increase Speed Decrease Cost

Plan

Change the Mechanism to Belt Pulley
• Ball screw if trying to increase speed => Belt mechanism may be more suitable => 1000mm/sec to 1500mm/sec is possible with the belt mechanism. Change to belt if there is no issue with positioning accuracy. • Reduce cost significantly if changing to belt is possible => Belt is inexpensive but its low rigidity may affect stability of servo motor operation, even with automatic tuning.

Belt Pulley Mechanism

Problems

1. Difference in Stopping Accuracy between Screw and Belt... How Much Stopping Accuracy Is Required?
2. Impact of Low Rigidity... Impact on Settling Time, Avoiding Tuning Problem

• Better stopping accuracy with the screw. No problem to change to the belt? => The application's required stopping accuracy is ±0.05 ~ 0.1mm, which is not as accurate as the one for the screw. Therefore, it should be okay to replace with the belt.
• If changing to the belt, rigidity on the mechanism gets low, thus the servo motor movements becomes unstable. => Among positioning motors, stepper motors do not have a built-in encoder. For this reason, they require no adjustment and are strong against low rigidity. Their movements are stable regardless of fluctuating loads. If the output is the same, consider stepper motors.

Estimation

Mechanism: Belt Pulley + Motor: Try with Stepper Motor

Stepper Motor vs Servo Mechanism Cost

• Transportable Mass -> Max. permissible load 7kg • Traveling Speed -> Improved to 800 mm/ sec Motor => By changing from stepper motor to servo motor, reduced cost by 50%! Mechanism => By changing from ball screw to belt mechanism, reduced cost by 7%!

Results

There Was Much Room for Cost Reduction!
By conducting a zero-based review of the mechanism as well as the motor selection based on characteristics, we managed to increase specifications and reduce cost, even with the motor size became slightly larger. In the past, motor selection was done based on its ease-of-use or familiarity. After this exercise, differences of operations between servo motors and stepper motors became clear. It was surprising that stepper motors are more affordable than expected. There must be room for cost reduction of other devices using this method. This exercise reacknowledged that the well-balanced selection between motor specifications and cost, while maximizing motor characteristics is the key.

Which Has Higher Stopping Accuracy - Stepper Motor or Servo Motor?

Customer Inquiry: Looking for a motor with good stopping accuracy. How much of a difference is there between stepper motors and servo motors?

Assumption: The AC servo motor NX Series is equipped with a 20-bit encoder, thus it should have a fine resolution, and good stopping accuracy.

First, it is necessary to clarify the difference between resolution and stopping accuracy: Resolution is the number of steps per revolution and it is also called a step angle for stepper motors. It is needed when considering how precise the required positioning needs to be. Stopping accuracy is the difference between the actual stop position and theoretical stop position.

Stepper Motor vs Servo Resolution and Stopping Accuracy

Does this mean that the AC servo motor equipped with a high accuracy encoder has better stopping accuracy than stepper motors?
Not quite. In the past there was no issue with the concept of "stopping accuracy of servo motors being equal to encoder resolution within ±1 pulse." However, recent servo motors are equipped with the 20 bit encoder (1,048,576 steps) which has a very fine resolution. Because of this, errors due to the encoder installation accuracy have a huge effect on stopping accuracy. Therefore, the concept of stopping accuracy has slightly started to change.
According to the comparison charts, stopping accuracy between stepper motors and AC servo motors is almost the same (±0.02º ~ 0.03º). Accuracy depends on the mechanical precision of the motor for stepper motors, thus if stop position can be done per 7.2º, positioning is done by the same small teeth on the rotor at all times, according to the motor structure. This makes it possible to further improve stopping accuracy.
However, stepper motors may generate displacement angle depending on the load torque value. Also, depending on the mechanism condition, AC servo motors may have wider hunting width as a response to gain adjustments. For these reasons, some caution is required.

Comparison of Stopping Accuracy Between Stepper Motors and AC Servo Motors

Stepper Motor vs Servo Stopping Accuracy

2-Phase Bipolar Stepper Motors
5-Phase Stepper Motors
Closed Loop Stepper Motors




©2025 - ORIENTAL MOTOR USA CORP. - All Rights Reserved